Other Parts Discussed in Thread: MSP430F2274, MSP-FET
Tool/software: TI C/C++ Compiler
Hi,
I've tried to use the crc_table function in the linker command file, but in the application I'm not able the calculate the same value as the Linker.
My development enviroment looks like:
Operating System: Windows 10 64Bit
CCS: 6.6.2
Compiler: TI MSP430 16.9.3 LTS
MCU: MSP430F2274
A snippet from the linker command file:
.TI.crctab : > FLASH
.cinit : {} > FLASH,PAGE=0,crc_table(_crc_table_cinit )
.const : {} > FLASH,PAGE=0,crc_table(_crc_table_const )
.text : {} > FLASH,PAGE=0,crc_table(_crc_table_text )
In the application I'm using the crc functions which are described in the document slaa221.pdf :
// CRC16 g(x) = x^16+ x^12 + x^5 + 1 (CCITT-Polynom).
// CCITT = CRC16_802_15_4
#define CRC16_802_15_4 1
#define CRC16_POLY 0x1021
#define CRC16_INIT_REM 0x0
#define CRC16_FINAL_XOR 0x0
unsigned int CRC_CheckROM(CRC_TABLE *tp) {
int i;
unsigned int uiResult = 0;
for (i = 0; i < tp->num_recs; i++) {
CRC_RECORD crc_rec = tp->recs[i];
if (crc_rec.crc_alg_ID == CRC16_802_15_4 ) // CRC_CCITT, CRC16_802_15_4 = 1
{
uint16_t uiCrc = 0;
uint16_t uiExpCrc = (uint16_t)crc_rec.crc_value; // expected checksum
unsigned char * pData = (unsigned char *) crc_rec.addr; // start address
// calculate the current checksum
uiCrc = CRC_CalcCRC16(CRC16_INIT_REM, CRC16_POLY, pData , crc_rec.size);
// Validate CRC Sum
if (uiCrc == uiExpCrc)
{
uiResult = 1; // pass
}
else
{
uiResult = 0; // fail
}
}
}
return uiResult;
}
unsigned short CRC_CalcCRC16(unsigned short crc, unsigned short poly,
unsigned char *pmsg, unsigned int msg_size)
{
unsigned int i, j;
unsigned short msg;
for(i = 0 ; i < msg_size ; i ++)
{
msg = (*pmsg++ << 8);
for(j = 0 ; j < 8 ; j++)
{
if((msg ^ crc) >> 15) crc = (crc << 1) ^ poly;
else crc <<= 1;
msg <<= 1;
}
}
return(crc ^ CRC16_FINAL_XOR);
}
I've implemted a table based crc function as well.
Here are my results:
.text section:
Linker: crc_value 0x00005A9E
Linker: crc_alg_ID 0x0001
Linker: addr 0x8000
Linker: size 0x1000
application:
16 Bit calculation bitwise: 0x1CBC
16 Bit table calculation: 0x1CBC
Where is my fault?
Kind regards,
Arne