This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28375D: TMS320F2837xD support the DWARF formats 2-4

Part Number: TMS320F28375D


Tool/software: Code Composer Studio

Hi TI Engineers,

I have a customer request which you can find the details below. Can you please provide an answer for the customer?

Thank you.

Customer's details;

"For our developments, we frequently use the DSPs of the C2000 series, currently the TMS320F2837xD and compile with the compiler TI v15.12.3.LTS. We would like to refer to the new compiler versions, e.g. v16.9.3.LTS. For the development, we use a self-made debugging tool, which relies on outfiles of type COFF, which finally expires with the newer compiler versions. Therefore, we want to rebuild our tool for the use with DWARF or build a parser from DWARF to COFF. The compiler supports DWARF 2 to 4. DWARF is constantly being developed, so it is foreseeable that a new version will be added every 2-5 years.
Now my question: are you planning to support the DWARF formats 2-4 in the future or will you follow the latest formats? We do not want to have to re-create our interface between outfile and tool every few years and therefore like to incorporate the development direction of TI in our planning."

Best regards,