This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: CCSV5.5

Tool/software: Code Composer Studio

Hai,

       I am working on LCDK6748 inorder to do image processing on CCSV5.5.I am unable to load image to CCSV5.5. Please help me 

  • Hi,

    There is very little information to make an educated guess to what may be happening in your case. Can you send some additional details?

    - Are you using a JTAG Debug Probe to connect to your LCDK board? You need one.
    - How are you configuring the Debug Probe to your LCDK inside CCS?
    - Are you able to connect to the C6748 core using CCS? If not, what are the error messages?
    - If you are able to connect, can you load code to your C6748 core? If not, what are the error messages?
    - If you are able to load code but unable to run, what are the error messages?
    - If the code seems to run fine but has an unexpected output, what is the expected output?

    Regards,
    Rafael

  • Hi,

    Given you opened many other threads after this post that showed progress, I assume the issues are solved and this thread will be closed.

    Regards,
    Rafael