This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC1310: ticloudagent.sh and libudev.so.0 on Debian

Part Number: CC1310


Tool/software: Code Composer Studio

Hi,

I'm using the web based CCS in firefox (it wouldn't work in chrome) on an up-to-date Debian/unstable system (Linux debian 4.16.0-1-amd64 #1 SMP Debian 4.16.5-1 (2018-04-29) x86_64 GNU/Linux).

However, I had to modify the ticloudagent.sh script to get it to work, so I'm reporting the changes here. Firstly, ldconfig is not typically in an unprivileged user's path, so it needs to be run as /sbin/ldconfig. And secondly, the line

LD_LIBRARY_PATH=$LD_LIBRARY_PATH:$CA_TEMPDIR

needs to be

export LD_LIBRARY_PATH=$LD_LIBRARY_PATH:$CA_TEMPDIR

in order for the LD_LIBRARY_PATH variable to be visible to the node command at the end of the file.

Cheers,

Brett.