This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMDSCNCD28335: Simulink cannot create CCS project - but

Part Number: TMDSCNCD28335


Tool/software: Code Composer Studio

1.

While using c2000 embedded coder toolbox, I successfully generate and download C-code to the control card using JTAG connector (XDS100 v3). The problem is that simulink cannot generate a project, and therefore I cannot open it in CCS for debugging and signal logging / plotting.

I have even uninstalled CCS v8 and installed v7 which should be supported. I still get this error message in Simulink.

"Unsupported CCS Version. Skipping CCS Project creation"

What should I do to make Simulink generate a CCS project?

2.

Signal logging does not work in Simulink, not even the example project. I've tried all COM ports and followed your guide. External mode should work with the XDS100 v3 right?

Any help is appreciated.