This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: DSS SCRIPT - TARGET IS NOT CONNECTED

Other Parts Discussed in Thread: TMS320C5505, CCSTUDIO

Tool/software: Code Composer Studio

Hi,

I'm trying to launch a program from command line using DSS.

I modified LoadProgram.js in the examples changing correctly variables deviceCCXMLFile and programToLoad for my purpose:

 

var deviceCCXMLFile = "C:\\Users\\marti\\Desktop\\BACKUP\\programmer\\targetConfigs\\TMS320C5505.ccxml";
var programToLoad = "C:\\Users\\marti\\Desktop\\\BACKUP\\DC2017\\project\\Debug\\DC2017_DEBUG.out";

when I launch DSS I have these exceptions:

C:\Users\marti>C:\TI\ccsv6\ccs_base\scripting\bin\dss.bat C:\TI\ccsv6\ccs_base\scripting\examples\DebugServerExamples\LoadProgram.js
SEVERE: Cannot perform operation, target is not connected.
SEVERE: Error loading "C:\Users\marti\Desktop\BACKUP\DC2017\project\Debug\DC2017_DEBUG.out": Cannot perform operation, target is not connected.
org.mozilla.javascript.WrappedException: Wrapped com.ti.ccstudio.scripting.environment.ScriptingException: Error loading "C:\Users\marti\Desktop\BACKUP\DC2017\project\Debug\DC2017_DEBUG.out": Cannot perform operation, target is not connected. (C:\TI\ccsv6\ccs_base\scripting\examples\DebugServerExamples\LoadProgram.js#26)
at org.mozilla.javascript.Context.throwAsScriptRuntimeEx(Context.java:1693)
at org.mozilla.javascript.MemberBox.invoke(MemberBox.java:160)
at org.mozilla.javascript.NativeJavaMethod.call(NativeJavaMethod.java:204)
at org.mozilla.javascript.optimizer.OptRuntime.call1(OptRuntime.java:66)
at org.mozilla.javascript.gen.c1._c0(C:\TI\ccsv6\ccs_base\scripting\examples\DebugServerExamples\LoadProgram.js:26)
at org.mozilla.javascript.gen.c1.call(C:\TI\ccsv6\ccs_base\scripting\examples\DebugServerExamples\LoadProgram.js)
at org.mozilla.javascript.ContextFactory.doTopCall(ContextFactory.java:340)
at org.mozilla.javascript.ScriptRuntime.doTopCall(ScriptRuntime.java:2758)
at org.mozilla.javascript.gen.c1.call(C:\TI\ccsv6\ccs_base\scripting\examples\DebugServerExamples\LoadProgram.js)
at org.mozilla.javascript.gen.c1.exec(C:\TI\ccsv6\ccs_base\scripting\examples\DebugServerExamples\LoadProgram.js)
at org.mozilla.javascript.tools.shell.Main.evaluateScript(Main.java:503)
at org.mozilla.javascript.tools.shell.Main.processFileSecure(Main.java:425)
at org.mozilla.javascript.tools.shell.Main.processFile(Main.java:391)
at org.mozilla.javascript.tools.shell.Main.processSource(Main.java:382)
at org.mozilla.javascript.tools.shell.Main.processFiles(Main.java:179)
at org.mozilla.javascript.tools.shell.Main$IProxy.run(Main.java:100)
at org.mozilla.javascript.Context.call(Context.java:528)
at org.mozilla.javascript.ContextFactory.call(ContextFactory.java:450)
at org.mozilla.javascript.tools.shell.Main.exec(Main.java:162)
at com.ti.ccstudio.apps.internal.scripting.RunScript$1.run(RunScript.java:88)
Caused by: com.ti.ccstudio.scripting.environment.ScriptingException: Error loading "C:\Users\marti\Desktop\BACKUP\DC2017\project\Debug\DC2017_DEBUG.out": Cannot perform operation, target is not connected.
at com.ti.debug.engine.scripting.Memory.loadProgram(Memory.java:932)
at sun.reflect.NativeMethodAccessorImpl.invoke0(Native Method)
at sun.reflect.NativeMethodAccessorImpl.invoke(NativeMethodAccessorImpl.java:57)
at sun.reflect.DelegatingMethodAccessorImpl.invoke(DelegatingMethodAccessorImpl.java:43)
at java.lang.reflect.Method.invoke(Method.java:606)
at org.mozilla.javascript.MemberBox.invoke(MemberBox.java:145)
... 18 more

It seems the target is not connected but it really is. In order to connect I use OLIMEX TMS320-XDS100-V3 device.

Any tip?

Thanks is advance

Paolo

  • i Solved by adding the line

    debugSession.target.connect();

    after the line
    debugSession = ds.openSession( ".*" );

    Please correct the example for the next release.

    Best Regards,
    Paolo
  • Paolo,

    I took a look at the examples in CCSv8. We don't have that exact example anymore but there is an equivalent one. I can see that it does have the explicit call to debugSession.target.connect(). I took a look at the example scripts from each release and it looks like this one was fixed in CCSv7.0.0.

    Thank you for reporting the issue.

    Regards,
    John