Part Number: TMS320F28069
Tool/software: Code Composer Studio
Hello,
My app is doing the following as a debug print about once every second:
sprintf((Uint8 *)&debug_string[0], "HRC1: H%lu, %lu, L%lu, %lu\r\n", xMessage.int_HRC1pulsewidthhigh0[i], xMessage.frac_HRC1pulsewidthhigh0[i], xMessage.int_HRC1pulsewidthlow0[i], xMessage.frac_HRC1pulsewidthlow0[i] );
USBBufferWrite((tUSBBuffer *)&g_sTxBuffer, (Uint8 *)&debug_string[0], strlen(debug_string));
I'm using the terminal in CCS to see the debug print - also - the app will run for a while and will eventually crash; usually hitting an ESTOP statement in an unhandled vector. (Only happens when I enable this debug priint output.)
The following is an example output: (<== marking the issue)
HRC1: H47, 61566, L48, 3970
HRC1: H61566, 47, L3970, 47 <==
HRC1: H47, 61566, L48, 3970
HRC1: H47, 63609, L48, 1927
HRC1: H47, 61682, L48, 3854
HRC1: H47, 61682, L48, 1927
HRC1: H47, 61682, L48, 3854
HRC1: H63609, 47, L3854, 47 <==
HRC1: H47, 63609, L48, 3854
HRC1: H47, 63609, L48, 1927
HRC1: H47, 61682, L48, 3854
HRC1: H47, 61682, L48, 3854
Any advice on this appreciated.
Thanks In Advance,
John