Part Number: TIDA-01281
Other Parts Discussed in Thread: TMS320F28035
Tool/software: Code Composer Studio
Hello Experts,
as stated in the title I have problems with the Olimex XDS100v3 in combination with the TMS320F28035 which is the controller of the TIDA-01281. I did all the adjustment mentioned in the manual (connection properties) of olimex and still getting the Error:
The JTAG IR and DR scan-paths cannot circulate bits, they may be broken.
An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault.
i've seen that this problem occurs often or at least I've found a lot of threads about this topic and all the including documents but I haven't found a solution yet. So I'd like to start at the beginning with the device manager:
- Is this what it is supposed to look like?
- Under target configs I've chosen the "Texas Instruments XDS100v3 USB Debug Probe_0". If I am corrent the emulator type is not available anymore. So this should be right?
- Next step for me would be checking the physical signals of the jtag. Is there anything significant? Pull-Ups/downs?
- Is it legitimately to check the "xclkout" to know whether the controller is working properly? Should I see a sine or a square clock?
Any further suggestions I could check or maybe a solution I have overlooked
Thank you very much
Best regards,
Thomas