This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CODECOMPOSER: CCS8 install MSP430Ware error

Part Number: CODECOMPOSER
Other Parts Discussed in Thread: MSP430WARE

Tool/software: Code Composer Studio

Hi,

I installed Code Composer Studio 8 in the fresh WIN10.

When I try to install MSP430Ware from Resource Explorer.

It shows error.

But SimpleLink MSP432 SDK is OK.

How do I do?

  • I have been trying to reproduce this on a couple of machines but have not had any luck.  For me it completes successfully.  One thing I noticed is that it is very slow to download.  Extracted it is almost 2GB.  The error message implies that there is a connection error and that is why it is failing.  The download should be getting mirrored to Taiwan.

    One thing that we could try is to download MSP430Ware from a different source and if that works Resource Explorer should detect it and just download the metadata for it.

    MSP430Ware can be downloaded from here:

    If you install in the standard location of C:\ti then Resource Explorer should detect it.  You can trigger it to scan by clicking on this menu:

    Regards,

    John

  • Hi John,

    Thank you, it's work!!!!

    YHH