This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: TI C/C++ Compiler
Hello
I'm using CCS v8 with Compiler C2000 Ti v18.1.1.
The compiler release v18.1.2 was updated from the beginning of May.
But I have not get a message from CCS that a new version of compiler was available.
So what is the update link to add in CCS to be checked automaticcaly by CCS?
Thank.
Hello
The link above is not the same where I found the v18.1.2.
From this link, it is available since the 3 may
http://software-dl.ti.com/codegen/non-esd/downloads/download.htm#C2000
C2000 Code Generation Tools v18.1.2.LTS [Windows] [Linux] [Mac OS X] |
Release Notes Closed Defects Open Defects |
May-03-2018. Bug |
But anyway, How be warned automaticcaly of new update? Because this make a long time CCS not warn me about new CCS and/or compiler release.
A GIR said:The link above is not the same where I found the v18.1.2.
From this link, it is available since the 3 may
http://software-dl.ti.com/codegen/non-esd/downloads/download.htm#C2000
Yes that link is fine also. Either link will work
A GIR said:But anyway, How be warned automaticcaly of new update? Because this make a long time CCS not warn me about new CCS and/or compiler release.
The issue is that the update site does not have 18.1.2 available for download. Once it is available there, then the CCS Update Manager will be aware of it. As for why it is not available, I don't know. I will see if I can get an answer for you
Thanks
ki