This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/UNIFLASH: uniflash command line to program mac address

Part Number: UNIFLASH


Tool/software: Code Composer Studio

Hi,

I am using UniFlash v4.3.1

I have to program MAC address through command line. I tried using UniFlash v3.4 and used the command

uniflash -ccxml <path to ccxml> -setOptions FlashMACAddrInput=AA-BB-CC-DD-EE-FF -operation ProgramMACAddress

It worked fine. But the command "operation" is not recognised in v4. What is the alternate command for this?

Can you please tell the command to program MAC address using UniFlash v4 ?

Regards

Sandra