Part Number: TMDSLCDK138
Tool/software: Code Composer Studio
CCS 7.4 / TMDSLCDK138 / TMS32-XDS100-V3
My build is stuck at 25% complete. It is "Invoking Command: C:\ti\ccsv7\utils\bin\gmake -k -j 8 all -O"
I thought it might be some sort of file locked from a previous build (because windows is so wonderful), so I rebooted, then did a "clean" and a "build".
Same deal, stuck at 25%.
Is there any way to get more visibility as to what's going on here?
I'd like to see the STDOUT from the build step so I can figure out what it's hung up on.