This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hi,
I'm working on the eCAN additional examples from the SPRA876. I imported all the 20 example projects to my workspace (CCS V7). But I'm having problems with 7 of them. When building, its said that :
warning: creating output section ".text" without a SECTIONS specification
warning: creating output section ".cinit" without a SECTIONS specification
warning: creating output section ".ebss" without a SECTIONS specification
warning: creating output section ".switch" without a SECTIONS specification
warning: creating output section ".adc_cal" without a SECTIONS specification
warning: creating output section "codestart" without a SECTIONS specification
warning: creating output section "ramfuncs" without a SECTIONS specification
warning: creating output section ".reset" without a SECTIONS specification
error: no valid memory range(NULL) available for placement of ".text"
error: program will not fit into available memory. placement with
alignment/blocking fails for section ".cinit" size 0x32 page 0. A
error: program will not fit into available memory. placement with
alignment/blocking fails for section ".switch" size 0x1e page 0.
error: program will not fit into available memory. placement with
alignment/blocking fails for section ".adc_cal" size 0x7 page 0.
error: program will not fit into available memory. placement with
alignment/blocking fails for section "ramfuncs" size 0x4 page 0.
error: program will not fit into available memory. placement with
alignment/blocking fails for section ".reset" size 0x2 page 0.
error: program will not fit into available memory. placement with
alignment/blocking fails for section "codestart" size 0x2 page 0.
The headers, .c source includes and DSP2833x_Headers_nonBIOS.cmd for all of the projects are from C:\ti\c2000\C2000Ware_1_00_04_00\device_support\f2833x
Yep. The projects that failed are: CAN_ECHO-AB; CAN_jig; CAN_TCOF_A; CAN_TRPRTSTP_A; CAN_TXABORT_A; CAN_TXLOOP_A & CAN_TXLOOP_B