This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28379D: Watch window CCS

Part Number: TMS320F28379D


Tool/software: Code Composer Studio

Hello community,

I made a program with Matlab/Simulink (2016b) and I load it on CCSv6.2. I've used the watch window to visualize my variables.

These are my questions:

  1. which variable should I pick from the .c file to visualize the ePWM generated?
  2. How can I visualize in the same graph (two or three) variables?
  3. When I try to visualize a sine wave, the graph obtained is as shown in the figure. Is there a particular configuration that I have to put forward?

Regards