Tool/software: TI-RTOS
Hi,
TI provides samples for the use of 2GHz radio communication with the CC1350 Launchpad (sample: rfWsnConcentrator, ...) and also the parallel use of 2GHz Link and BLE advertisement (sample: rfWsnDmConcentrator). I am interested in building a GATT server that works parallel to the 2GHz radio link (BLE GATT server provides the data received by radio communication). There are no sample for such task, but there is an standalone sample for the establishement of a GATT server with the CC1350 Launchpad (Sample: SimplePeripheral).
Can rfWsnDmConcentrator (or rfWsnConcentrator) be combined with the SimplePeripheral sample? Or how a such implementation can be done (in Code Composer Studio)?
Regards,
Mazen