Part Number: TMS320F28235
Tool/software: TI C/C++ Compiler
Hi,
Customer faced an compiler issue on F28235, about function calls issue.
The compiler version is V4.1.3, very old version.
In code1.c file, function func(int, int) is defined, and it is called in another file code2.c like func(DEFINE_1, DEFINE_2).
DEFINE_1 and DEFINE_2 are macro. Inside, there are global parameters add operation.
After calling func(DEFINE_1, DEFINE_2), customer found that, DEFINE_2's value was not passed into the function correctly. Its value was 0. DEFINE_1's value was passed successfully.
What' could be the issue?
Thanks in advance.
Br, Jordan