Other Parts Discussed in Thread: OMAPL138
Tool/software: TI C/C++ Compiler
Hello,
I am using OMAPL138 for my project. For DSP (C6748), I developed a C++ CCS 6.1.3 project with compiler version 7.4.16 in linux virtual machine. In compiler options, Debug options-> Debugging model , there are different options to choose and one is blank. I want to choose blank option for optimization , but when I try to select it, it always comes out with
symbolic debug for program analysis (default) (--symdebug:skeletal)
option. The same thing I do in windows version of CCS , It can choose blank option. Even it works for CCS 5.5 of linux virtual machine.
Anyone can verify this for linux Virtual machine for CCS version 6.1.3?
Thanks,
Rushina.