Part Number: TMS320C5515
Tool/software: Code Composer Studio
Hi,
I have a project for the C5515 which was created in code composer v6.x.
I have it imported into a new computer running Code Composer v8.1.0.00011.
I have the TI v4.4.1 compiler downloaded and installed now (I wasn't initially aware it didn't come with version v8 of Code Composer).
When I click the build button for my project nothing happens, there is no output from the compiler in the output window, nothing.
It is as if the IDE never sent the project to the compiler.
I noticed my imported project never has the project name in bold when selected too (see attached picture).
However, if I make a new project from scratch in v8 of Code Composer it will be sent for compilation when the build button is pushed.
Thanks,
Ben