Other Parts Discussed in Thread: TM4C1290NCPDT
Tool/software: Code Composer Studio
I did a clean install of CCS 6.1,2 on a lab PC and I went through the steps I normally go through to install CCS on other PC’s I have successfully used in the past. The tools are set up to build for a Tiva TM4C1294NCPDTCPU. After CCS was installed and set up, I created a new project / simple hello world project in a new directory off the root of the C drive called delme and the directory I created a new workspace folder and new project folder so everything is clean as far as the new project I create.
The build fails because it is looking in the path C:\Users\myuserName\AppData\Local\Temp\ as you can see in the compiler output in bold below. I have no idea what is pointing to C:\Users\l235766\AppData\Local\Temp\ but that is what I think the problem is. I thought that installing CCS would fix it since you can have multiple versions of CCS installed on a PC without affecting each other.
I assume the problem is something in the PC but I don't know what it could be. The PC is windows XP.
Thanks,
Doug
**** Build of configuration Debug for project mtProj ****
"C:\\ccs6p1p2\\ccsv6\\utils\\bin\\gmake" -k all
subdir_rules.mk:7: recipe for target 'main.obj' failed
process_begin: CreateProcess(C:\Users\l235766\AppData\Local\Temp\make547532-1.bat, C:\Users\l235766\AppData\Local\Temp\make547532-1.bat, ...) failed.
make (e=2): The system cannot find the file specified.
gmake: *** [main.obj] Error 2
subdir_rules.mk:14: recipe for target 'tm4c1290ncpdt_startup_ccs.obj' failed
process_begin: CreateProcess(C:\Users\l235766\AppData\Local\Temp\make547532-2.bat, C:\Users\l235766\AppData\Local\Temp\make547532-2.bat, ...) failed.
make (e=2): The system cannot find the file specified.
gmake: *** [tm4c1290ncpdt_startup_ccs.obj] Error 2
gmake: Target 'all' not remade because of errors.
**** Build Finished ****