Part Number: MSP430F167
Tool/software: TI C/C++ Compiler
As part of a MSP430F167 code development process the .out file from CCS was disassembled by dis430.exe.
A "designed to be stand alone code section" was then inspected for any calls/jumps outside the stand alone code's defined address range.
Earlier versions of the MSP430 disassembler (dis430.exe) produced hex addresses in the disassembly, but later versions replaced the hex addresses with their symbolic names.
For example the early disassemblers would produce this format
009840: B012 CALL #0xbe48
But the later ones produce this format
009852: B012 CALL #set_hw_rev
dis430.exe -h shows there is an option
--noaddr,-a Do not print ADDRESS with label names within instructions
Which I read as reverting the output to the old format, but I can't get it to produce the old format.
Is there a way to have the newer versions of dis430.exe to produce the old hex format without the symbols inserted?
Thanks,
John Wright