Hi all,
In CCSv4 I was trying to invoke some user-defined GEL functions (which involved memory read), while the CPU is still running. These GEL functions do not work (get stalled), if the CPU is running. In CCSv4, the GEL functions work only when the CPU is halted.
However, in case of CCS v3.3 I was able to invoke GEL functions at run-time. I am using CCSv4 (version: 4.0.0.16001) and I like to whether this feature of invoking GEL functions at run-time is supported in any of the latest versions of CCSv4.
Thanks,
Karthik.