This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TMS570LC4357: compilation issue ti_cgt_arm 181.2 LTS , for generic files

Part Number: TMS570LC4357

Tool/software: Linux

While compiling from Linux in ti_cgt_arm 181.2 LTS compiler, the genric function for eg:- Floor()-{which is coming from math.h file ,and we have included the math.h file in the source code} , for that we are getting unresolved symbol error.

 Can you please check why it is coming.

  • I am unsure whether you see the error diagnostic when compiling, or linking.  

    If you see the diagnostic while compiling, then for the source file that sees the error, please send in a test case as described in the article How to Submit a Compiler Test Case.

    If you see the diagnostic while linking, then please show exactly how the linker is invoked, along with all the resulting diagnostics.  I might be able to understand the problem from that information alone.  However, I may have to ask you send in the entire project.

    Thanks and regards,

    -George