Part Number: CC2640R2F
Tool/software: Code Composer Studio
I've found that pretty often (several times per hour), while I am paging through code, CCS 8 will freeze up for a second or two, and then resume. If I look at it in Win 10 task manager during the lag, it is taking a full load of one of my CPU cores. I'm pretty new to CCS so I can't say if this is expected behavior for CCS. Apart from these incidents, CCS is pretty responsive.
I noticed in the CCS tips & tricks, it is noted that workspaces can get corrupted, and to rebuild them occasionally. Is this one of the signs I need to rebuild the workspace?
Any other ideas - if it is not the workspace?