Part Number: TM4C129ENCPDT
Tool/software: Code Composer Studio
Hello,
I have been trying to port some of embedded programs from windows development to linux development. Unfortunately, even though I am using all of the same libraries and compilers. The ndk library I use has some differences when it is compiled in Windows Vs Linux. I am trying to understand why this difference exists, its significance, and finally if I can remove it so that the files are functionally the same. An example difference is in the stk_nat_ppp_pppoe file. By comparing the files using objdiff from cgxml-2.61.00, I get the following difference:
objdiff linux\stk_nat_ppp_pppoe.aem4f windows\stk_nat_ppp_pppoe.aem4f ofd6x Processing linux\stk_nat_ppp_pppoe.aem4f ... Processing windows\stk_nat_ppp_pppoe.aem4f ... Comparing files ... ********************************************************************** Filename sock.oem4f ********************************************************************** ====================================================================== Comparing Sections : section = .text:SockShutdown : elf32_shdr ====================================================================== Differences: linux\stk_nat_ppp_pppoe_02.aem4f windows\stk_nat_ppp_pppoe.aem4f sh_size: 0x70 0x7c Files are different
For reference, here is the relevant tool-chain information:
Target: ti.targets.arm.elf.M4F
Compiler: ti-cgt-arm_5.2.6
XDC tools: xdctools_3_31_01_33_core
SYSBIO version: bios_6_42_03_35