Part Number: LAUNCHXL-CC2640R2
Tool/software: Code Composer Studio
Hi, I developed a BLE application, originally base on project zero, using CCS_7.3. It works fine! Now I trying to merge it to CCs_8.10.00011. Everything seems to compile ok but when I go for 'debug' I get the following output in the 'console' after download the *.out file:
Cortex_M3_0: GEL Output: Memory Map Initialization Complete.
Cortex_M3_0: GEL Output: Board Reset Complete.
Cortex_M3_0: Symbol Manager: the object file contains invalid call frame information at .debug_frame 0x5d32; the rest of call frame information will be skipped. Callstack may not be unwound properly.
Please advise
kind regards,
Laurent