Using CCSv5 version N201010041800. Want to see power/clock status as in: http://processors.wiki.ti.com/index.php/ICEPICK#Q:_How_do_I_see_the_ICEpick_registers_in_CCS_v4.3F on OMAP3.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Using CCSv5 version N201010041800. Want to see power/clock status as in: http://processors.wiki.ti.com/index.php/ICEPICK#Q:_How_do_I_see_the_ICEpick_registers_in_CCS_v4.3F on OMAP3.
Hi Steve,
You can find the target status view in CCSv5, select Windows | Show Views in the main window and look for the Target Status view in the list.
Regards,
Patrick
Steve,
Another thing that you will need to do is to enable display of routers in debug view. Once you have them showing, then you will see status once icepick is connected. This is something that we are hoping of resolving for LR update.
Easiest way of enabling display of routers is(in my opinion) start a debug sessions, select top node, right click and choose "Edit targetConfigName.." ; then choose first tab and enable "Routers" checkbox on right hand side. Click Apply/Continue and restart debug session.
Martin
Thanks Martin, I think I made it almost work. I wasn't able to get just the router to show up, but after checking all items (routers, daps, etc.) and restarting, I was able to make it show. I connected to just the ICEpick, but then I didn't get any status in the properties box that shows me power and clock. I attached my screen shot.
Can you update the wiki at: http://processors.wiki.ti.com/index.php/ICEPICK#Q:_How_do_I_see_the_ICEpick_registers_in_CCS_v4.3F to reflect how to do this for v5?

Hi Steve,
Power and Clock is a property of the subpath of the icepick, you have to connect to one of the core to see the subpath properties in the Target Status view.
Regards,
Patrick
Patrick, we should be able to get the subpath property by only connecting to ICEpick (i.e. connect to ICEpick and NOT connect to core yet).
With V5, even when connected to the core, it still doesn't show the power/clock status.

Steve,
Can you let me know the version of CCSv5 that you are using? I was able to see the status in my enviornment.
Regards,
Patrick
I see the problem in the build that you are using. I have confirmed this issue was resolved 2 weeks ago and will be available in future service release.
Regards,
Patrick