This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CCSTUDIO: Pre-Processor command text options

Part Number: CCSTUDIO


Tool/software: Code Composer Studio

Hello,

I'm using CCS 8.1 to write some assembly with a MSP430 processor.

I was wondering if CCS provides anyway to customize the pre-processor commands that allow conditional assembly? Specifically CCS makes text after '|' (bitwise OR) green like a comment so chaining $defined s looks ugly/confusing

Thanks!

  • Jacob,

    There is unfortunately only a limited amount of syntax coloring options available in CCS for assembly source files and your request is not one of them.

    The issue with text that comes after '|' being highlighted as a comment is a known issue (see related thread here). However, we inherit the editor from Eclipse and unfortunately there hasn't been an easy way for us to provide our own fix for this. So I don't see a short term fix for this. Sorry about the inconvenience caused due to this.

  • Okay, that's unfortunate but it is what it is. Thanks for the timely response!