Tool/software: Code Composer Studio
Hi,
We're happily using CCS 6.1.3.00033 to develop with the 2812, 28035, 28335, and 6713.
I'm wondering if we should upgrade our installations (we have about 8 users) to version 8 just to be up to date. I'm tempted to stay where we are, because everything is stable and we all know all the ins and outs of this version. But I've seen places where version 6 is referred to as "very old".
1) Are we missing out on anything by staying at 6.1.3.00033 ? Our code is in the 20,000 lines range for each project so compilation time isn't an issue.
2) The 6713 is a very old part, we had to downgrade the compiler to find one that works. Would we be able to use it with a newer CCS?
3) Can version 8 coexist with 6.1.3.00033?
Thanks for any input,
Lloyd