It is giving other Errors now.
Description Resource Path Location Type
gmake: Target 'all' not remade because of errors. Example_2833xAdcToDMA C/C++ Problem
gmake: *** [Example_2833xAdcToDMA.out] Error 1 Example_2833xAdcToDMA C/C++ Problem
errors encountered during linking; "Example_2833xAdcToDMA.out" not null: errors encountered during linking; "Example_2833xAdcToDMA.out" not Example_2833xAdcToDMA C/C++ Problem
cannot find file "rts2800_fpu32_fast_supplement.lib" null: cannot find file "rts2800_fpu32_fast_supplement.lib" Example_2833xAdcToDMA C/C++ Problem
null: entry-point symbol other than "_c_int00" specified: "code_start" Example_2833xAdcToDMA C/C++ Problem
Invalid project path: Include path not found (\V100\include). Example_2833xAdcToDMA pathentry Path Entry Problem
Invalid project path: Include path not found (\packages\ti\xdais). Example_2833xAdcToDMA pathentry Path Entry Problem
Build-variable 'XDAIS_CG_ROOT' cannot be resolved. This project may not build as expected. Example_2833xAdcToDMA properties Problem
Build-variable 'INSTALLROOT_2833X_TO_FASTRTS' cannot be resolved. This project may not build as expected. Example_2833xAdcToDMA properties Problem