This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS4 for 32bit with Keil MDK 32 bit compatibility

Hi,

One of my customers has Keil MDK for 8bit, 16 bit and 32 bit versions on his PC. Because of the licensing method of Keil, he is not able to use the 32 bit version of Keil and 16 bit version on the same machine. He is currently buying CCS4 to code the C2000. He will be installing the IDE on the same machine as the Keil. We want to make sure that there is no compatibility issue with using the Keil and CCS together. Please share your views if you have faced any issue before.

  • Santhosh,

    There should be no issues with having CCSv4 and Keil installed on the same computer.  I had the both installed for a while last year and did not have any problems.  The are separate applications and don't share any drivers.

     

    Regards,

    John