This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software: Code Composer Studio
Hi ,
I am using 6713.When I connect to PC via external jtag emulator it is showing in device manager that blackhawk usb 2.0 JTAG emulator.It is not there in my ccsv5.5 .So,how to download that emulator in ccsv5.5
The Blackhawk drivers get installed as part of the CCS installation, however this emulator is from a different manufacturer, not Blackhawk. I am not familiar with it and would suggest checking with the manufacturer for the appropriate drivers.
The emulator is probably a clone of the discontinued Blackhawk XDS510-Class "USB 2.0 JTAG Emulator" (sites such as ebay have these clones with various different branding on the case).sai krishna vemaraju99 said:I am using 6713.When I connect to PC via external jtag emulator it is showing in device manager that blackhawk usb 2.0 JTAG emulator.
According to USB 2.0 JTAG Emulator (BH-USB-2) support in Code Composer 4 the "USB 2.0 JTAG Emulator" is only supported under CCSv4.1.2 or earlier.