Part Number: TMS320F28377S
Tool/software: Code Composer Studio
I am posting this for my customer:
I am trying to build the Buck_VMC_F2837xS project but it is throwing me an error stating “program will not fit”. The error is on line 115 of F2837xS_FLASH_DP_BoosterPack.CMD file.
It also shows the following warnings:
“This project was created using a version of compiler that is not currently installed - 6.4.2 [C2000]. Another version of the compiler will be used during build - 18.1.2.LTS.”
“This project was created using a version of XDCtools that is not currently installed: 3.31.0.22_core_eng. Please install the XDCtools of this version, or migrate the project to one of the supported versions.”
I used power suite (from control suite) to access the example project and CCS (Version: 8.1.0.00011) to compile it. The Buck_VMC-Main.c file is created on June 2015 and version is 1.0
Please advise possible solutions for these roadblocks.