Part Number: TMS320VC5416
Tool/software: Code Composer Studio
Hello,
I have been trying to connect to my old custom board equipped with a TMS320VC5416 using - Code Composer Studio v5.2, Blackhawk 560-USB-v2 System trace emulator and CCXML file and selecting the TMS320C5416 since there is no TMS320VC5416 in the selection menu.while performing a "Test connection" I get the picture that my signal integrity is just fine since all the Tests run successfully, and there is no problem on either the Debugger's side or the Target's side. When i try to "Launch selected configuration" using my CCXML File it manages to connect and suspends the Processor but I am not able to read any of the registers or view disassembly of the target even after Connected-Suspended. sometimes when i connect the registers would show they're all 0x0000 which doesn't make sense.. and if that doesn't happen then it's written "Unable to read data" in red font. same goes for the disassembly.. I either get a spam of the same command or it just says it was unable to read the data memory from this address (It applies basically to all addresses). I have read about the Security ROM/RAM modes that this Device can implement but I never knew or never tried to Lock and activate these modes.. Could i have accidentally made it secure without even knowing and now I can't connect at all to my device? I'd like to get some help from you guys if anyone has ever bumped across a situation such as this.
Hopefully even Ki-So-Lee comes to rescue me from this situation as well ;D
Thank you very much in advance! =]