This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F2806: Warning on Wrong line

Part Number: TMS320F2806


Tool/software: Code Composer Studio

Hello,

At the project we a building I am receiving a warning as follows:

As can be seen, the warning refers to line 566, when actually the line is at 568, and when I insert parenthesis as recommended

the system doesn't recognize this fix, and when using the automatic fix at lines 565 or 567 is inserts parenthesis in those lines instead.

I have tried cleaning and rebuilding the project which didn't change the situation.

Besides, this solution and project run on two different computers which use the same project and configuration via perforce file controlling system.

(after reading their instructions about which files should be put in their depot when using CCS).

In my colleagues computer this warning doens't appear at all.

Any help will be appreciated,

Thanks,

Amitai