This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Not able to run cc_setup.exe

I installed 4.1.x and then downloaded/installed an update (4.2.0.10017). I do not have a cc_setup icon on my desktop (I might have deleted it, the one I deleted was a v3.3 setup). I tried to add a shortcut on my desktop to the C:\Program Files\Texas Instruments\ccsv4\DebugServer\bin\win32\cc_setup.exe but when I try to run I get an error "This app has failed to start because CCReg.dll was not found. Re-installing the app may fix this problem". I didn't want to reinstall because then I would have to download the update which took quite a while.

Any ideas?