This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320C6748: UIA Sysem Analyser takes too much of processor's time

Part Number: TMS320C6748
Other Parts Discussed in Thread: OMAP-L138, , SYSBIOS

Tool/software: Code Composer Studio

Hello,

I'm working with Blackhawk USB 560 v2 System Trace debugger and transferring log data using UIA system analyser in runtime mode.

I used the article https://e2e.ti.com/support/development_tools/code_composer_studio/f/81/p/614025/2262772#2262772   to make it work.

But unfortunately it seems that it eats to much of the processor's resources. When I open Rtos Analyser -> Printf and Error logs or Load Analysis while the project of voice exchange from/to codec is running, CPU load reaches up to 100% and some gaps in speech in the output occur. If I change LoggingSetup.loggerType  from  LoggingSetup.LoggerType_JTAGRUNMODE to LoggingSetup.LoggerType_STOPMODE all the gaps disappear and CPU load on "CPU Load: graph" decreases to 70-80 %.

Is it possible to decrease CPU load in run-time mode?

Best regards,

Egor.