Part Number: TSC2000
Tool/software: Code Composer Studio
I am unable to install CCSv8 on my machine, I get an error related to TCL, here is the bitrock_installer log. I am on a Windows 10 machine.
Thank you,
Paul
_____________________________________________________________________________________________________________________
Log started 08/23/2018 at 13:41:08
Preferred installation mode : unattended
Trying to init installer in mode unattended
Mode unattended successfully initialized
[13:41:08] Found mode
Executing \\witfs01\Shared\Engineering\EmbeddedSystemsGroup\Tools\TI\CCS_8_0_0\ccs_setup_8.0.0.00016.exe --mode win32 &
Script exit code: 0
Script output:
Script stderr:
[13:41:10] Unable to delete previously generated bitrock files.
[13:41:10] Windows 10 0
[13:41:10] installer_command_line_arguments :
[13:41:10] installer_command_line_arguments :
[13:41:10] Product Name Code Composer Studio 8.0.0
[13:41:10] Product Version 8.0.0.00016
[13:41:10]
Preparing to Install
Preparing to Install
Unpacking files
Unpacking files
Unpacking files
Extracting compressed file C:\Users\paul.das\Local Settings\ofview-x64.zip
File is locked. Failed to overwrite C:/Users/paul.das/Local Settings//util/ofview-x64.zip
Error copying file from C:/Users/paul.das/Local Settings//util/ofview-x64.zip/ofview-x64.zip to C:/Users/paul.das/Local Settings//util/ofview-x64.zip:
C:/Users/paul.das/Local Settings//util/ofview-x64.zip/ofview-x64.zip does not exist
Unable to copy file
Unpacking files
Unpacking files
Unpacking files
Unpacking files
[13:41:13] admin = 1
[13:41:13] installertype = setup
[13:41:13] ccsinstaller_name ccs_setup_8.0.0.00016.exe
[13:41:13] Installer: \\witfs01\Shared\Engineering\EmbeddedSystemsGroup\Tools\TI\CCS_8_0_0/ccs_setup_8.0.0.00016.exe
[13:41:13]
[13:41:13] running C:\Users\paul.das\Local Settings/ccs_a7e5d697-b078-4edd-76c6-eeb642909807\tcl\bin\tclsh "C:/Users/paul.das/Local Settings/ccs_a7e5d697-b078-4edd-76c6-eeb642909807/installer_tcl/main_frontend/main.tcl" --installersrc "//witfs01/Shared/Engineering/EmbeddedSystemsGroup/Tools/TI/CCS_8_0_0" --installertmp "C:/Users/paul.das/Local Settings/ccs_a7e5d697-b078-4edd-76c6-eeb642909807" --buildid 8.0.0.00016 --installer "//witfs01/Shared/Engineering/EmbeddedSystemsGroup/Tools/TI/CCS_8_0_0/ccs_setup_8.0.0.00016.exe" --bitness 64-bit --os windows --osname "Windows 10" --spversion "0" --timestamp 20180823134110 --AVon false --tl false
Executing C:\Users\paul.das\Local Settings/ccs_a7e5d697-b078-4edd-76c6-eeb642909807\tcl\bin\tclsh "C:/Users/paul.das/Local Settings/ccs_a7e5d697-b078-4edd-76c6-eeb642909807/installer_tcl/main_frontend/main.tcl" --installersrc "//witfs01/Shared/Engineering/EmbeddedSystemsGroup/Tools/TI/CCS_8_0_0" --installertmp "C:/Users/paul.das/Local Settings/ccs_a7e5d697-b078-4edd-76c6-eeb642909807" --buildid 8.0.0.00016 --installer "//witfs01/Shared/Engineering/EmbeddedSystemsGroup/Tools/TI/CCS_8_0_0/ccs_setup_8.0.0.00016.exe" --bitness 64-bit --os windows --osname "Windows 10" --spversion "0" --timestamp 20180823134110 --AVon false --tl false
Script exit code: 1
Script output:
Script stderr:
application-specific initialization failed: Can't find a usable init.tcl in the following directories:
{C:/Users/paul.das/Local Settings/ccs_a7e5d697-b078-4edd-76c6-eeb642909807/tcl/lib/tcl8.6} {C:/Users/paul.das/Local Settings/ccs_a7e5d697-b078-4edd-76c6-eeb642909807/tcl/lib/tcl8.6} {C:/Users/paul.das/Local Settings/ccs_a7e5d697-b078-4edd-76c6-eeb642909807/lib/tcl8.6} {C:/Users/paul.das/Local Settings/ccs_a7e5d697-b078-4edd-76c6-eeb642909807/tcl/library} {C:/Users/paul.das/Local Settings/ccs_a7e5d697-b078-4edd-76c6-eeb642909807/library} {C:/Users/paul.das/Local Settings/ccs_a7e5d697-b078-4edd-76c6-eeb642909807/tcl8.6.6/library} {C:/Users/paul.das/Local Settings/tcl8.6.6/library}
This probably means that Tcl wasn't installed properly.
couldn't read file "C:/Users/paul.das/Local Settings/ccs_a7e5d697-b078-4edd-76c6-eeb642909807/installer_tcl/main_frontend/main.tcl": no such file or directory
Error running C:\Users\paul.das\Local Settings/ccs_a7e5d697-b078-4edd-76c6-eeb642909807\tcl\bin\tclsh "C:/Users/paul.das/Local Settings/ccs_a7e5d697-b078-4edd-76c6-eeb642909807/installer_tcl/main_frontend/main.tcl" --installersrc "//witfs01/Shared/Engineering/EmbeddedSystemsGroup/Tools/TI/CCS_8_0_0" --installertmp "C:/Users/paul.das/Local Settings/ccs_a7e5d697-b078-4edd-76c6-eeb642909807" --buildid 8.0.0.00016 --installer "//witfs01/Shared/Engineering/EmbeddedSystemsGroup/Tools/TI/CCS_8_0_0/ccs_setup_8.0.0.00016.exe" --bitness 64-bit --os windows --osname "Windows 10" --spversion "0" --timestamp 20180823134110 --AVon false --tl false: application-specific initialization failed: Can't find a usable init.tcl in the following directories:
{C:/Users/paul.das/Local Settings/ccs_a7e5d697-b078-4edd-76c6-eeb642909807/tcl/lib/tcl8.6} {C:/Users/paul.das/Local Settings/ccs_a7e5d697-b078-4edd-76c6-eeb642909807/tcl/lib/tcl8.6} {C:/Users/paul.das/Local Settings/ccs_a7e5d697-b078-4edd-76c6-eeb642909807/lib/tcl8.6} {C:/Users/paul.das/Local Settings/ccs_a7e5d697-b078-4edd-76c6-eeb642909807/tcl/library} {C:/Users/paul.das/Local Settings/ccs_a7e5d697-b078-4edd-76c6-eeb642909807/library} {C:/Users/paul.das/Local Settings/ccs_a7e5d697-b078-4edd-76c6-eeb642909807/tcl8.6.6/library} {C:/Users/paul.das/Local Settings/tcl8.6.6/library}
This probably means that Tcl wasn't installed properly.
couldn't read file "C:/Users/paul.das/Local Settings/ccs_a7e5d697-b078-4edd-76c6-eeb642909807/installer_tcl/main_frontend/main.tcl": no such file or directory
[13:41:14] CCS_ERROR: Installer exited with error code
[13:41:14]
[13:41:14] application-specific initialization failed: Can't find a usable init.tcl in the following directories:
{C:/Users/paul.das/Local Settings/ccs_a7e5d697-b078-4edd-76c6-eeb642909807/tcl/lib/tcl8.6} {C:/Users/paul.das/Local Settings/ccs_a7e5d697-b078-4edd-76c6-eeb642909807/tcl/lib/tcl8.6} {C:/Users/paul.das/Local Settings/ccs_a7e5d697-b078-4edd-76c6-eeb642909807/lib/tcl8.6} {C:/Users/paul.das/Local Settings/ccs_a7e5d697-b078-4edd-76c6-eeb642909807/tcl/library} {C:/Users/paul.das/Local Settings/ccs_a7e5d697-b078-4edd-76c6-eeb642909807/library} {C:/Users/paul.das/Local Settings/ccs_a7e5d697-b078-4edd-76c6-eeb642909807/tcl8.6.6/library} {C:/Users/paul.das/Local Settings/tcl8.6.6/library}
This probably means that Tcl wasn't installed properly.
couldn't read file "C:/Users/paul.das/Local Settings/ccs_a7e5d697-b078-4edd-76c6-eeb642909807/installer_tcl/main_frontend/main.tcl": no such file or directory
There has been an error.
No origin file found that matched C:/Users/paul.das/Local Settings//bitrock_installer.log