Other Parts Discussed in Thread: DRV8301
Tool/software: Code Composer Studio
I AM GETTING THIS ERROR
Description Resource Path Location Type
#1965 cannot open source file "sw/modules/math/src/32b/math.h" main.c /TRY line 2 C/C++ Problem
HERE COMPLETE PROGRAM IS GIVEN
// modules
#include "sw/modules/math/src/32b/math.h"
#include "sw/modules/memCopy/src/memCopy.h"
#include "sw/drivers/can/src/32b/f28x/f2806x/can.h"
#pragma DATA_SECTION(ECanaRegs,"ECanaRegsFile");
volatile struct ECAN_REGS ECanaRegs;
#pragma DATA_SECTION(ECanaMboxes,"ECanaMboxesFile");
volatile struct ECAN_MBOXES ECanaMboxes;
volatile struct ECAN_REGS ECanaShadow;
// drivers
// platforms
#include "main.h"
// **************************************************************************
// the defines
#define LED_BLINK_FREQ_Hz 5
// **************************************************************************
// the globals
uint_least32_t gLEDcnt = 0; // Counter used to divide down the ISR rate for visually blinking an LED
HAL_Handle halHandle; // Handle to the Inverter hardware abstraction layer
USER_Params gUserParams; // Contains the user.h settings
HAL_PwmData_t gPwmData = {0,0,0}; // Contains PWM duty cycles in global Q format
HAL_AdcData_t gAdcData = {0,0,0,0,0,0,0}; // Contains Current and Voltage ADC readings in global Q format
volatile MOTOR_Vars_t gMotorVars = MOTOR_Vars_INIT;
#ifdef FLASH
// Used for running BackGround in flash, and ISR in RAM
extern uint_least16_t_t *RamfuncsLoadStart, *RamfuncsLoadEnd, *RamfuncsRunStart;
#endif
#ifdef DRV8301_SPI
// Watch window interface to the 8301 SPI
DRV_SPI_8301_Vars_t gDrvSpi8301Vars;
#endif
uint_least32_t ErrorCount;
uint_least32_t PassCount;
uint_least32_t MessageReceivedCount;
uint_least32_t TestMbox1 = 0;
uint_least32_t TestMbox2 = 0;
uint_least32_t TestMbox3 = 0;
int i,j;
long loopcount = 0;
int MBX_data[32]; // This array stores the data to be transmitted
// **************************************************************************
// the functions
// Prototype statements for functions found within this file.
void mailbox_check(int_least32_t T1, int_least32_t T2, int_least32_t T3);
void mailbox_read(int_least16_t i);
void InitECana(void);
void main(void)
{
uint_least16_t j;
MessageReceivedCount = 0;
ErrorCount = 0;
PassCount = 0;
struct ECAN_REGS ECanaShadow;
// Only used if running from FLASH
// Note that the variable FLASH is defined by the project
#ifdef FLASH
// Copy time critical code and Flash setup code to RAM
// The RamfuncsLoadStart, RamfuncsLoadEnd, and RamfuncsRunStart
// symbols are created by the linker. Refer to the linker files.
memCopy((uint_least16_t_t *)&RamfuncsLoadStart,(uint_least16_t_t *)&RamfuncsLoadEnd,(uint_least16_t_t *)&RamfuncsRunStart);
#endif
// initialize the hardware abstraction layer
halHandle = HAL_init(&hal,sizeof(hal));
// check for errors in user parameters
USER_checkForErrors(&gUserParams);
// store user parameter error in global variable
gMotorVars.UserErrorCode = USER_getErrorCode(&gUserParams);
// do not allow code execution if there is a user parameter error
if(gMotorVars.UserErrorCode != USER_ErrorCode_NoError)
{
for(;;)
{
gMotorVars.Flag_enableSys = false;
}
}
// initialize the user parameters
USER_setParams(&gUserParams);
// set the hardware abstraction layer parameters
HAL_setParams(halHandle,&gUserParams);
#ifdef LAUNCHPAD
// Setup GPIOs 0 and 1 as outputs for use in project lab1 only.
// This is specific to the launchpad because its LEDs are also used by the PWM channels.
HAL_setupLaunchPadGpio0and1(halHandle);
#endif
// setup faults
HAL_setupFaults(halHandle);
// initialize the interrupt vector table
HAL_initIntVectorTable(halHandle);
// enable the ADC interrupts
HAL_enableAdcInts(halHandle);
// enable global interrupts
HAL_enableGlobalInts(halHandle);
// enable debug interrupts
HAL_enableDebugInt(halHandle);
// disable the PWM
HAL_disablePwm(halHandle);
#ifdef DRV8301_SPI
// turn on the DRV8301 if present
HAL_enableDrv(halHandle);
// initialize the DRV8301 interface
HAL_setupDrvSpi(halHandle,&gDrvSpi8301Vars);
#endif
InitECana();
ECanaMboxes.MBOX0.MSGID.all = 0x9555AAA0;
ECanaRegs.CANMD.bit.MD0 = 0 //0 -> Tx 1 -> Rx
// Enable all Mailboxes */
// Since this write is to the entire register (instead of a bit
// field) a shadow register is not required.
ECanaShadow.CANME.all = ECanaRegs.CANME.all;
ECanaShadow.CANME.all = 0xFFFFFFFF;
ECanaRegs.CANME.all = ECanaShadow.CANME.all;
ECanaMboxes.MBOX0.MSGCTRL.bit.DLC = 8;
EALLOW;
/************** comment out part **************/
/*ECanaRegs.CANMIM.all = 0xFFFFFFFF;
// Configure the eCAN for self test mode
// Enable the enhanced features of the eCAN.
EALLOW;
ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
ECanaShadow.CANMC.bit.STM = 1; // Configure CAN for self-test mode
ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
EDIS;*/
for(;;)
{
ECanaMboxes.MBOX0.MDL.all = 12345678;
ECanaMboxes.MBOX0.MDH.all = 0x89ABCDEF;
ECanaRegs.CANTRS.bit.TRS0 = 1;
while(ECanaRegs.CANTA.bit.TA0 != 1 ) {} // Wait for all TAn bits to be set..
ECanaRegs.CANTA.bit.TA0 = 1; // Clear all TAn
for(j=0; j<1; j++) // Read & check 16 mailboxes
{
mailbox_read(j); // This func reads the indicated mailbox data
mailbox_check(TestMbox1,TestMbox2,TestMbox3); // Checks the received data
}
}
interrupt void mainISR(void)
{
// toggle status LED
if(gLEDcnt++ > (uint_least32_t)(USER_ISR_FREQ_Hz / LED_BLINK_FREQ_Hz))
{
HAL_toggleLed(halHandle,(GPIO_Number_e)HAL_Gpio_LED2);
gLEDcnt = 0;
}
// acknowledge the ADC interrupt
HAL_acqAdcInt(halHandle,ADC_IntNumber_1);
// convert the ADC data
HAL_readAdcData(halHandle,&gAdcData);
// ADC processing and pwm result code goes here
// write the PWM compare values
HAL_writePwmData(halHandle,&gPwmData);
return;
} // end of mainISR() function
void mailbox_read(int_least16_t MBXnbr)
{
volatile struct MBOX *Mailbox;
Mailbox = &ECanaMboxes.MBOX0 + MBXnbr;
TestMbox1 = Mailbox->MDL.all; // = 0x9555AAAn (n is the MBX number)
TestMbox2 = Mailbox->MDH.all; // = 0x89ABCDEF (a constant)
TestMbox3 = Mailbox->MSGID.all;// = 0x9555AAAn (n is the MBX number)
} // MSGID of a rcv MBX is transmitted as the MDL data.
void mailbox_check(int_least32_t T1, int_least32_t T2, int_least32_t T3)
{
if((T1 != T3) || ( T2 != 0x89ABCDEF))
{
ErrorCount++;
}
else
{
PassCount++;
}
}
void InitECana(void) // Initialize eCAN-A module
{
/* Create a shadow register structure for the CAN control registers. This is
needed, since only 32-bit access is allowed to these registers. 16-bit access
to these registers could potentially corrupt the register contents or return
false data. */
struct ECAN_REGS ECanaShadow;
EALLOW; // asm(" asm(" EALLOW")") enables access to protected bits
/* Configure eCAN RX and TX pins for CAN operation using eCAN regs*/
ECanaShadow.CANTIOC.all = ECanaRegs.CANTIOC.all;
ECanaShadow.CANTIOC.bit.TXFUNC = 1;
ECanaRegs.CANTIOC.all = ECanaShadow.CANTIOC.all;
ECanaShadow.CANRIOC.all = ECanaRegs.CANRIOC.all;
ECanaShadow.CANRIOC.bit.RXFUNC = 1;
ECanaRegs.CANRIOC.all = ECanaShadow.CANRIOC.all;
/* Configure eCAN for HECC mode - (reqd to access mailboxes 16 thru 31) */
// HECC mode also enables time-stamping feature
ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
ECanaShadow.CANMC.bit.SCB = 1;
ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
/* Initialize all bits of 'Message Control Register' to zero */
// Some bits of MSGCTRL register come up in an unknown state. For proper operation,
// all bits (including reserved bits) of MSGCTRL must be initialized to zero
ECanaMboxes.MBOX0.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX1.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX2.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX3.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX4.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX5.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX6.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX7.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX8.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX9.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX10.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX11.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX12.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX13.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX14.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX15.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX16.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX17.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX18.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX19.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX20.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX21.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX22.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX23.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX24.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX25.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX26.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX27.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX28.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX29.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX30.MSGCTRL.all = 0x00000000;
ECanaMboxes.MBOX31.MSGCTRL.all = 0x00000000;
// TAn, RMPn, GIFn bits are all zero upon reset and are cleared again
// as a matter of precaution.
ECanaRegs.CANTA.all = 0xFFFFFFFF; /* Clear all TAn bits */
ECanaRegs.CANRMP.all = 0xFFFFFFFF; /* Clear all RMPn bits */
ECanaRegs.CANGIF0.all = 0xFFFFFFFF; /* Clear all interrupt flag bits */
ECanaRegs.CANGIF1.all = 0xFFFFFFFF;
/* Configure bit timing parameters for eCANA*/
ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
ECanaShadow.CANMC.bit.CCR = 1 ; // Set CCR = 1
ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
// Wait until the CPU has been granted permission to change the configuration registers
do
{
ECanaShadow.CANES.all = ECanaRegs.CANES.all;
} while(ECanaShadow.CANES.bit.CCE != 1 ); // Wait for CCE bit to be set..
ECanaShadow.CANBTC.all = 0;
/* The following block is for 80 MHz SYSCLKOUT. (40 MHz CAN module clock Bit rate = 1 Mbps
See Note at end of file. */
ECanaShadow.CANBTC.bit.BRPREG = 1;
ECanaShadow.CANBTC.bit.TSEG2REG = 4;
ECanaShadow.CANBTC.bit.TSEG1REG = 13;
ECanaRegs.CANBTC.all = ECanaShadow.CANBTC.all;
EALLOW;
ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
ECanaShadow.CANMC.bit.CCR = 0 ; // Set CCR = 0
ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
// Wait until the CPU no longer has permission to change the configuration registers
do
{
ECanaShadow.CANES.all = ECanaRegs.CANES.all;
} while(ECanaShadow.CANES.bit.CCE != 0 ); // Wait for CCE bit to be cleared..
/* Disable all Mailboxes */
ECanaRegs.CANME.all = 0; // Required before writing the MSGIDs
//EDIS;
}
PLEASE solve the issue