This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LabView shares data with CCS?

Hi, everyone:

I have an experimental kit F28335 and on-board emulator XDS100V2. When debugging, the CCS collects data from DSP through XDS100, which doesn't support RTDX.

As real-time property is not important for me, so I needn't use an special communication interface, for example SCI.Then letting Labview shares data with CCS is the most economic method for me.

So is there some other way for Labview to reuse the data that DSP sents to host computer? Maybe it is too simple for you, but just give me some hint.

Thanks

Qian

  • Hi everyone,

    I am also facing the same problem of whether DSP Test Integration Toolkit by National Instruments is supported by CCSv4. I have used the toolkit previously with CCSv3.3. However, the VI which is used for opening the project in CCSv3.3 asks for a path to the .pjt files. Can the projects in CCSv4 saved as .pjt files in some way? Then I can attempt to open the project using the aforementioned NI toolkit.

    Regards,

    Debarati.