Tool/software: Code Composer Studio
We have a usecase to automate device initialization on one of our Sitara devices, where to simplify the device initialization process, we would like to run a DSS script when customer launches the connection using their target configuration file? without this feature, customers have the additional step to run this script from the console on every reset and also need to make sure that the DSS script points to their target configuration file location. Having this option will address both the issues.
Is this possible/supported with CCSv8 ? Does a DSS script always have to be run from Scripting console or are their hooks to launch the script from GEL or from .ccxml?
Appreciate your inputs and support on this topic.
Regards,
Rahul