Part Number: MSP-EXP430G2
Tool/software: Code Composer Studio
Hi, I'm using both 64-bit CCS 8.1.0 on my 64-bit Windows 10 computer and the CCS cloud to work with my MSP-EXP430G2 launchpad.
While debugging the C code, I had a few things in mind.
0. Is there a link from TI that describes the difference between CCS's SW/HW breakpoints?
1. Using the basic serial debugger which is on the launchpad, how many SW/HW breakpoints can I set while debugging?
I think there are limits to place those.
2. When using the CCS cloud version, does this limitation applies as well?
3. If I use a different debugger, like TMS320-XDS100-V3, or a different microcontroller/launchpad, such as the TM4C Tiva series,
will the breakpoint limit will change?