This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F280049: TMS320F280049

Part Number: TMS320F280049


Tool/software: Code Composer Studio

Hello,

I installed Code Composer Studio 8.1, but it looks like it is only recognizing the ARM processor targets. I can’t figure out how to add C2000 targets from the documentation. Any suggestions?

Thank you,

Errol

  • Hello Errol,
    Looks like you are missing C2000 device support. You can re-run the installer on top of your existing installation to add components that you missed during that initial installation.

    For an example, see the below video:
    www.youtube.com/watch

    The above video is for an older CCS version but the concept in the same - the installer was re-run on top of an existing installation.

    Thanks
    ki