Part Number: TMS320C6455
Tool/software: TI C/C++ Compiler
Hi
DSP: C6455
CCS: 5.3 (3.3)
Board:
OS: Win7 for 5.3, XP for 3.3
When I declared a global variable in my program, the program hanged when DSP want to connect ethernet!!!!. (DSP connect to ethernet and program worked correctly before I declared a global variable)
After debugging I find out that when I set the optimization level of a program file to " O3 " the problem happened.
The file that I changed the optimization level was my parser faile(DSP parsed the received data from ethernet).
When I set the optimization level to Non or O2 the all the things works correctly, I mean I declared a global variable and DSP connect to ethernet and there is not any problem.
Why did this problem happen? Please guide me
BR