Part Number: DRV8303
Other Parts Discussed in Thread: CONTROLSUITE,
Tool/software: TI C/C++ Compiler
Hello,
recently in my possession came DRV8303EVM board and i am trying to establish connection between Code Composer Studio and board through USB port, i have installed CCS and controlsuite on my computer, also i have downloaded software from the official site (DRV8303EVM_C200_FIRMWARE).
The problem that i am getting error that the system can not find the specified path for the xds100-f28035.ccxml, When i make a new .ccxml file and start debugging session, error pops up that connection cannot be establish over USB.
Is there some steps that are missing and do i need to use older compiler (Ti v18.1.3.LTS) to compile this project ?
In User's Guide SLVU983A–September 2013–Revised October 2013 step 16 is where the error pops up...
Thanks Ivan