Part Number: TMS320C6474
Tool/software: Code Composer Studio
Hi,
I am trouble reading values and expression in real-time from CCS on c6474 using debugger. The program says "Error: Could not read <address>: Execution state prevented access". I have looked around the forum for similar issues, and found out that the problem is because the DSP is running in free running state. A fix for this is check "Halt the target before any debugger access'' in the project's debug properties.
But unfortunately, I cannot use active project based debug session. I need to use a non-project based debug session and read some variables. There is no option for halting the target when opening a debug session using .ccxml file. Is there a workaround for this..? I need to open a non-project debug session, load symbols and then read some variables all while not halting the system. TY.