Other Parts Discussed in Thread: BLE-STACK, CC2640
Tool/software: TI C/C++ Compiler
Hi All
I have a case need to upgrade stack4.0 to stack4.2.
I have two versions of CCS(7.4 and 8.1) in different PC.
Then add "pargma NOINIT" in the glucose sample code of stack 4.0 & 4.2
In stack 4.0 is success.(sample code not modified)
In Stack 4.2, glucose sample code, CCS7.4 & 8.1
<main.c>
#pragma NOINIT (GLUValue)
uint8_t GLUValue;
.......
int main()
{
RegisterAssertCback()
PIN_init()
ICall_init()
ICall_createRemoteTask()
GAPRole_createTask()
GLUValue = 1; <== if have assign value, The program will stop in create task.
GlucoseSensor_createTask()
BIOS_start()
return 0;
}
<glucose.c>
GlucoseSensor_createTask(void)
{
.........
Task_construct(&glucoseTask, GlucoseSensor_taskFxn, &taskParams, NULL); <== stop here(CCS 7.4 & 8.1 are the same )
}
---------------------------
Have tried to tune the optimization leve on CCS. The same situation.
What should I do?