Part Number: TMS320F28335
Tool/software: Code Composer Studio
New user here and I'm attempting to get an XDS510 USB PLUS emulator working with CCSv7 and a F28335 control card (release 2.2) which is inserted into the TI Docking-Stn USB-EMU. Until now I've been using the onboard USB JTAG emulator on the docking station without a problem, but now I need to connect to it via JTAG so I can prepare for the prototype boards.
Clicking on the debug icon results in the error...
Error connecting to the target:
(Error 102 @ 0x0)
Internal error: Invalid error code. Restart the application. If error persists, please report the error.
(Emulation package 7.0.48.0)
I have the following config under Project->Properties->CCS General->Configuration->Main
Family: C2000
Variant: < > TMS320F28335
Connection: Spectrum Digital XDS510USB Emulator TI-JSC
My colleague has CCSv5 with Spectrum Digital XDS510USB-PLUS Emulator via JSC (which I don't see in my list of options) and he doesn't have any connectivity issues.
Does the option I have selected "...XDS510USB Emulator TI-JSC" include the XDS510USB-PLUS?
Is there anything else I should be looking at to work past this issue?
I've also tried SDConfigEX XDS510USB->510 Emulator-Test and it detects 1 JTAG device in the scan chain