Tool/software: Code Composer Studio
I seem to be getting closer. I am getting a linker error indicating a library cannot be found. But, the library file is in a path that is included in the link command line:
Building target: "C:/OBVP-GCBR/THAAD/CODE/Control DSP/CP_FLASH/../Debug/T4_CP_Build.out"
Invoking: C2000 Linker
"C:/ti/ccsv8/tools/compiler/ti-cgt-c2000_18.1.2.LTS/bin/cl2000" -v28 -ml -mt --advice:performance=all --define=_DEBUG --define=LARGE_MODEL -g --diag_wrap=off --display_error_number --c_src_interlist --asm_directory="C:/OBVP-GCBR/THAAD/CODE/Control DSP/Debug" --obj_directory="C:/OBVP-GCBR/THAAD/CODE/Control DSP/Debug" -z -m"C:/OBVP-GCBR/THAAD/CODE/Control DSP/Debug/T4_CP_Build.map" --stack_size=0x400 --warn_sections -i"C:/OBVP-GCBR/THAAD/CODE/Control DSP/lib/Flash2812_API_V210/lib" -i"C:/ti/ccsv8/tools/compiler/ti-cgt-c2000_18.1.2.LTS/lib" -i"C:/OBVP-GCBR/THAAD/CODE/Control DSP/CP_FLASH" -i"C:/OBVP-GCBR/THAAD/CODE/Control DSP" -i"C:/ti/ccsv8/tools/compiler/ti-cgt-c2000_18.1.2.LTS/include" --reread_libs --diag_wrap=off --display_error_number --xml_link_info="CP_FLASH_linkInfo.xml" --rom_model -o "C:/OBVP-GCBR/THAAD/CODE/Control DSP/CP_FLASH/../Debug/T4_CP_Build.out" "C:/OBVP-GCBR/THAAD/CODE/Control DSP/Debug/app_AngSpeed.obj" "C:/OBVP-GCBR/THAAD/CODE/Control DSP/Debug/app_BIT.obj" "C:/OBVP-GCBR/THAAD/CODE/Control DSP/Debug/app_FOC.obj" "C:/OBVP-GCBR/THAAD/CODE/Control DSP/Debug/app_Fault.obj" "C:/OBVP-GCBR/THAAD/CODE/Control DSP/Debug/app_HWS.obj" "C:/OBVP-GCBR/THAAD/CODE/Control DSP/Debug/app_ISR.obj" "C:/OBVP-GCBR/THAAD/CODE/Control DSP/Debug/app_MsgProcessor.obj" "C:/OBVP-GCBR/THAAD/CODE/Control DSP/Debug/app_PI.obj" "C:/OBVP-GCBR/THAAD/CODE/Control DSP/Debug/bsp_adc.obj" "C:/OBVP-GCBR/THAAD/CODE/Control DSP/Debug/bsp_can.obj" "C:/OBVP-GCBR/THAAD/CODE/Control DSP/Debug/bsp_canC.obj" "C:/OBVP-GCBR/THAAD/CODE/Control DSP/Debug/bsp_flash.obj" "C:/OBVP-GCBR/THAAD/CODE/Control DSP/Debug/bsp_isr.obj" "C:/OBVP-GCBR/THAAD/CODE/Control DSP/Debug/bsp_pwm.obj" "C:/OBVP-GCBR/THAAD/CODE/Control DSP/Debug/bsp_sci.obj" "C:/OBVP-GCBR/THAAD/CODE/Control DSP/Debug/bsp_spi.obj" "C:/OBVP-GCBR/THAAD/CODE/Control DSP/Debug/bsp_sysctrl.obj" "C:/OBVP-GCBR/THAAD/CODE/Control DSP/Debug/bsp_timers.obj" "C:/OBVP-GCBR/THAAD/CODE/Control DSP/Debug/global.obj" "C:/OBVP-GCBR/THAAD/CODE/Control DSP/Debug/main.obj" "C:/OBVP-GCBR/THAAD/CODE/Control DSP/Debug/vector.obj" "C:/OBVP-GCBR/THAAD/CODE/Control DSP/CP_FLASH.cmd" "C:/OBVP-GCBR/THAAD/CODE/Control DSP/lib/Flash2812_API_V210/lib/Flash2812_API_V210.lib" "C:/OBVP-GCBR/THAAD/CODE/Control DSP/lib/IQmath/v15a/lib/IQmath.lib" -lrts2800_ml.lib -llibc.a
<Linking>
"C:/OBVP-GCBR/THAAD/CODE/Control DSP/CP_FLASH.cmd", line 66: error #10008-D: cannot find file "Flash2812_API_V210.lib"
"C:/OBVP-GCBR/THAAD/CODE/Control DSP/CP_FLASH.cmd", line 67: error #10008-D: cannot find file "Flash2812_API_V210.lib"
The library file “Flash2812_API_V210.lib” is located in folder “C:/OBVP-GCBR/THAAD/CODE/Control DSP/lib/Flash2812_API_V210/lib”.
Also, I unchecked “ XDAIS” in the Products tab and checked the “XDCtools” and I get the following warnings. Is this a problem?
Description Resource Path Location Type
Build-variable 'XDAIS_CG_ROOT' cannot be resolved. This project may not build as expected. CP_FLASH properties Problem
Invalid project path: Include path not found (\packages\ti\xdais). CP_FLASH pathentry Path Entry Problem
Invalid project path: Include path not found (C:\OBVP-GCBR\THAAD\CODE\include). CP_FLASH pathentry Path Entry Problem
Thanks for your help!