This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS570LS3137: Not able to compile the ASM files in the CCS7 [E0002] Illegal mnemonic specified & [E0000] Unrecognized special character

Part Number: TMS570LS3137

Tool/software: Code Composer Studio

When i am trying to compile the complete project which contains C-Source files along with the ASM files But i am not able to compile only the ASM files but the c-source files are compiled. Below are the Error details coming for the ASM files

Error Description:

Description Resource Path Location Type
[E0000] Unrecognized special character abc.asm /Shetty/02_SW/SRC line 18 C/C++ Problem

Description Resource Path Location Type
[E0002] Illegal mnemonic specified abc.asm /Shetty/02_SW/SRC line 1 C/C++ Problem

Compiler Used: Ti v15.12.4 LTS

Code Composer Studio Version: 7.3.0.00019

Regards,

Narasimha Setty Bapur