This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Cycle Accurate Simulator is not?

I am getting different CLK high resolution timer results depending on whether the code runs on the emulator hardware, or various "cycle accurate" simulators.

ccs 4.1.2.00027, DSP/BIOS 5.41.02.14, c6748 300 MHz

I setup a simple 20ms PRD then run statistics using the CLK high resolution timer.

When I run on the emulator hardware I get 6,000,000 ticks between interrupts which is exactly what you would expect. 
When I run on the C6747 Device Cycle Accurate SImulkator I get 3,000,000 ticks between interrupts. 
When I run on the C674x Cycle Accurate SImulator I get 3,857,371 ticks between interrupts. 

All three sources return 300,000 ticks per ms when I call CLK_countspms().  Obviously at least one of them is wrong...